Transitions
Transitions are represented by small horizontal bars that cross the connection link. Each transition is referenced by a name, written next to the transition symbol. This information is called the level 1 of the transition.
When using single divergences, the first transitions following the divergence are set in a group to define their priority of execution. The priority of transitions is automatically assigned and follows the order of creation of the divergence branch. Specify a different priority for a transition. The possible priority values range from 1 to 255. The higher value indicates the higher priority.

TIP:
For transitions following divergences, set the
priorities in the Properties window for transitions. Access by right-clicking the transition
or the title bar of the transition's level 2.
To insert a transition
- From theToolbox, drag the transition element into the language container.
- To link the transition to an existing step, click the mouse with the cursor on the grid cell above or below the step.
- Specify a different priority for a transition following a divergence:
- Right-click the transition, and then clickProperties.
- In thePropertieswindow, set the priority to the required value, and then clickOK.
- (optional) To renumber the steps and transitions, from theToolsmenu, point toMulti-language Editor, and then clickRenumber Steps and Transitions.
Provide Feedback