SFC Elements
When working in Sequential Function Chart (SFC) programs, insert these elements. A program always has an initial step.
- Steps
- Transitions
- Sequence Controls
- Jumps to Steps
When inserting steps and transitions, these are assigned a default naming convention including numbering. For steps, the default naming is Sn where S indicates a step and n indicates the numbering for the step. For transitions, the default naming is Tn where T indicates a transition and n indicates the numbering for the transition. Rename steps and transitions. However, when renaming steps and transitions using the default naming convention and changing only the numbering, renumber these elements to a numbering scheme starting from top to bottom, then from left to right.
Before Renumbering | After Renumbering |
|---|---|
![]() | ![]() |
To renumber steps and transitions
Renumbering ignores steps and transitions using a naming convention other than the default Sn for steps and Tn for transitions.
- Open the SFC program for which to renumber the steps and transitions.
- From theToolsmenu, point toMulti-language Editor, and then clickRenumber Steps and Transitions.
Provide Feedback