Jumps to Steps
Jump symbols indicate a connection link from a transition to a step, without having to draw
a connection line. Reference the jump symbol with the name of the destination step:
A Jump symbol cannot represent a link from a step to a transition.
![]() | Jump to Step S1 |
Example
These charts are equivalent. The chart on the left uses links to return from the bottom to
the top of the chart while the chart on the right uses jumps to return to the top of the
chart.


To insert a jump to a step
- From theToolbox, drag the jump element into the language container and place it directly below the existing transition.
- In theSelect Destination Stepdialog box, select the required step and then clickOK.The jump is displayed in the language container.
Provide Feedback