Coding Conditions for Transitions

Code conditions for clearing of transitions by programming these in the level 2 window. Only one condition can be attached to a transition. When changing the programming language of a transition, the code zone must be empty. When defining the properties of conditions, indicate a name, priority, comment (optional), and the programming language (type). The available programming languages for transitions are Ladder Diagram (LD) and Structured Text (ST).
When no expression is attached to the Transition, the default condition is TRUE.
To code conditions for transitions
  1. Select the transition for which to code a condition.
  2. Right-click the transition, then choose
    Properties
    .
  3. Specify the required properties for the transition from the
    Properties
    window.
    1. To rename the transition, type the required text in the Name field.
    2. To specify the type (programming language) for the transition condition, choose the required type in the
      Type
      field.
    3. To include a comment, type the required text in the
      Comment
      field.
  4. In the Level 2 window, program the required condition.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal