Conditions Programmed in LD

Describe the condition attached to a transition with the Ladder Diagram (LD) language. A diagram can have only one rung and one coil. The coil, to which a variable cannot be assigned, represents the activation status of the transition. Add blocks and contacts to define the logic.
Example
(* SFC Program with LD programming for transitions *)
sfc_cpld1
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal