Starting and Stopping Controllers
Stop an AADvance controller while it runs. Also start a stopped AADvance controller. Start or stop individual controllers or all controllers in a project. Starting or stopping a controller is only available when the controller is disconnected. For individual controllers, view the version information and the current status and any comments.

To start or stop controllers
- Disconnect from the running controllers.TIP: Starting or stopping a controller that has restricted access, that is, when another user is debugging a project in the controller, does not execute the start or stop command.
- From the Project menu, click Start/Stop.The Start/Stop Application dialog box displays.
- In the Start/Stop Application dialog box, set one of the following actions for each controller:
- None
- Start
- Stop
- Click Apply. A warning displays to confirm the actions. Click OK.
The applications running on the AADvance controllers stop or start.
Provide Feedback