Connect with controllers
Connect with the physical controllers when developing an application. A virtual machine executes the code for each controller in real-time on the equipment.
TIP:
Breakpoints, cycle-to-cycle, and step-by-step execution
are only available while simulating an application.
Connect individual controllers within a project. Use the
Connect
dialog box to
select individual or all controllers. When connected, perform tasks that include:- Monitor program execution and the values of variables
- Lock and unlock I/O channels of an I/O module
- Modify values of variables
- Modify cycle timingIMPORTANT:
- When connected, do not modify any controllers. Modifications may be lost after disconnecting.
- Connecting to multiple controllers after a library update uses the library content that matches the topmost selected controller from theConnectdialog box. TheConnect In Progressdialog box may warn that some libraries may not match the running application for other controllers. To use library content that matches another controller, connect only to that controller.
When connected, a local or remote
AADvance-Trusted SIS Workstation software
locks a controller from other users while performing any operation modifying the controller. Only one AADvance-Trusted SIS Workstation software
can lock a controller at any given time. Operations that lock a controller include performing downloads and updates, modifying the values of variables and I/Os, modifying cycle timing, and more. The AADvance-Trusted SIS Workstation software
unlocks access after disconnecting from the controller or after completing a download. When the AADvance-Trusted SIS Workstation software
locks a controller, the identity is indicated as the user name from the computer. If the AADvance-Trusted SIS Workstation software
is unable to restrict access to the controller, the operation modifying the controller fails.
TIP:
Check in all pending changes before connecting.
Status information for a controller appears as a lightning bolt icon in the
Application View
, Communication View
, and Equipment View
:Icon | Description |
|---|---|
![]() | Yellow. Controller is unlocked and available to any AADvance-Trusted SIS Workstation software . |
![]() | Green. Controller is locked by a local AADvance-Trusted SIS Workstation software and unavailable from other AADvance-Trusted SIS Workstation software . |
![]() | Red. Controller is locked by a remote AADvance-Trusted SIS Workstation software and unavailable to local AADvance-Trusted SIS Workstation software . |
![]() | Grey. Controller is not connected or is in simulation mode. |
From these views, obtain detailed status information for controllers including the identity of an
AADvance-Trusted SIS Workstation software
locking a controller by mousing over the controller status icons. The Controller Status
displays the identities of AADvance-Trusted SIS Workstation software
locking controllers.
IMPORTANT:
Before initially connecting to controllers, build
the project, then download the code to the controller. Subsequent connections automatically
extract the controller code from the version control repository resulting from the latest
download or update operation.
To connect with controllers
- In theCommunication View, specify the IP addresses for the controllers in the project.The compiler generates different code for simulation than for targets.
- From theProjectmenu, point toConnect Mode, and then clickOnline.TheOnlinemenu category appears with the online command options.
- Build the controller or project code.
- Download the code to the physical controller or controllers.
- In theApplication View, select the controller or project to connect, then from theOnlinemenu clickConnect(or pressF5).
- In theConnectwindow, select the controller or controllers to connect, and then clickConnect.The selected controllers are connected.
Provide Feedback