Disconnecting from Controllers

For a project, disconnect all running controllers executing applications. Before downloading code to controllers or clearing applications from controllers, disconnect controllers.
TIP: Disconnecting from a controller does not restore the project folder to the same state before it connected to the controller. If cleaning the project before connecting to a controller, clean the project again after disconnecting from the controller.
To disconnect controllers
  1. In the
    Application View
    , select the controller or project.
  2. In the
    Online
    menu, click
    Disconnect
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal