Download code to controllers
Download project code to the physical controllers. No download is required to simulate an application.
Prerequisites:
- Connect the computer where theAADvance-Trusted SIS Workstation softwareis installed to the hardware controller through an SNCP network.
- Fit the program enable key into theAADvance® Control Systemcontroller.
- Set theCode for Simulationproperty to True for all controllers.
- Set the value of theSFC States Mem Sizeproperty to reserve sufficient space for SFC program organization units (POUs).TIP: To change the resource number of a controller, clear the application from theAADvance Control Systemcontroller. Modify the resource number inAADvance Discoverand in theAADvance Control Systemcontroller properties, then download the code to theAADvance Control Systemcontroller.
When downloading code, the
AADvance-Trusted SIS Workstation software
verifies that the latest build
reflects the current project.
TIP:
If unable to download an
application to a controller, free memory by clearing the applications from the
AADvance Control System
controller.When unable to connect to a
AADvance Control System
controller with a valid IP address:- Cancel the update or download in progress and then retry the operation.
- Verify that the resource number specified in the AADvance project is correct usingAADvance Discover.
To download code to controllers
- Clean the project.
- Build the project code.
- Verify the program enable key is plugged into the key connector on the 9100 processor base unit.
- From theApplication View, right-click the project, and then clickDownload.
- In theDownloadwindow, select the controllers, and then clickDownload.TheAADvance-Trusted SIS Workstation softwarechecks in the controllers to download into the version source control repository, then downloads the code to the physical controllers. TheAADvance-Trusted SIS Workstation softwareapplies a label to the controller in the source control repository for each successful download.
Provide Feedback