Clearing an Application
Previously downloaded applications may be cleared from a physical controller. For a project, choose to clear either individual controllers or all controllers. Applications may only be cleared from disconnected controllers. Replace an application in an AADvance controller by clearing the controller and then downloading a new application.
When clearing applications, specify the individual controllers from those existing in a project, then specify the controllers to clear applications. For individual controllers, view version information for the local and physical controller applications, status of the controller, and any comments.
TIP:
When clearing an application, only the files for the
current resource number are deleted. It is recommended to clear the application before
changing resource number.
To clear an application
- Disconnect from the running controllers.
- In theApplication View, select the project, then from theProjectmenu, clickClear.
- In theClear Applicationdialog box, perform one of the following:
- To clear applications for individual controllers, select the required controllers, and then clickClear.
- To clear applications for all controllers, clickSelect All, and then clickClear.
The application files are removed from the required physical controllers. Now download a different application with the same IP address to the physical controller.
Provide Feedback