Variable Cross References
In the element list, color is used to identify elements used within the project. Elements displayed as blue are used at least once within the project. Elements displayed as red are not in use. For elements other than programs, select elements displayed as blue to view the location information for each instance of the element within the project. Jump to the location of individual instances by double-click in the instance list.
Properties for the Variables view are:
Property | Description |
|---|---|
Name | Name of the variable |
Scope | Range of accessibility of a variable in relation to program organization units (POUs) of a controller |
Alias | Alias name of the variable |
Type | Data type of the variable |
Project | Project using the variable |
Controller | Controller using the variable |
Comment | Comment of the variable |
Group | Group containing the variable |
Provide Feedback