Function and Function Block Cross References
In the element list, color is used to identify elements used within the project. Elements displayed as blue are used at least once within the project. Elements displayed as red are not in use. For elements other than programs, select elements displayed as blue to view the location information for each instance of the element within the project. Jump to the location of individual instances by double-click in the instance list.
Properties for the Functions and Function Blocks views are:
Property | Description |
|---|---|
Name | Name of the function or function block |
Category | Type of function or function block. Possible types are standard, user-defined, and native. |
Language | Programming language of the function or function block |
Project | Project using the function or function block |
Controller | Controller using the function or function block |
Comment | Comment of the function or function block |
From Library | Library containing the function or function block |
Provide Feedback