Defined Word Cross References
In the element list, color is used to identify elements used within the project. Elements displayed as blue are used at least once within the project. Elements displayed as red are not in use. For elements other than programs, select elements displayed as blue to view the location information for each instance of the element within the project. Jump to the location of individual instances by double-click in the instance list.
The properties for the Defined Words view are:
Property | Description |
|---|---|
Name | Name of the defined word |
Equivalent | String replacing the defined word during compilation. For example, the defined word "PI" is replaced by its equivalent "3.14159" |
Project | Project using the defined word |
Comment | Comment for the defined word |
Provide Feedback