Program Cross References
In the element list, color is used to identify elements used within the project. Elements displayed as blue are used at least once within the project. Elements displayed as red are not in use. For elements other than programs, select elements displayed as blue to view the location information for each instance of the element within the project. Jump to the location of individual instances by double-click in the instance list.
Properties for the Programs view are:
Property | Description |
|---|---|
Name | Name of the program |
Language | Programming language of the program |
Project | Project using the program |
Controller | Controller using the program |
Comment | Comment of the program |
Provide Feedback