Intelligent Update Manager
To access the Intelligent Update Manager
- From theBuildmenu, clickIntelligent Update Manager.
When intelligent updates are enabled, the Intelligent Update Manager dialog box displays a list of target snapshots after the initial compilation. Snapshots are copies of application versions taken after a download. Set the number of historical snapshots saved by the Intelligent Update Manager using the Intelligent Update Options dialog box. When the maximum number of historical snapshots is exceeded, the oldest snapshot is deleted. Protect snapshots. Protected snapshots are not included in the maximum number of historical snapshots. Also delete snapshots.

Unless specified otherwise, the newest snapshot is set as the current target snapshot. The current target snapshot has a gray background and is the topmost item in the list. A snapshot is necessary for intelligent updates to function properly.
TIP:
Obtain application version information from the
TIC
Version Checker
or from the Diagnostic Tool
.The
Intelligent Update Manager
compares the most recently compiled application with the target snapshot version currently running on the target and attempts to match data points and values between both. The Intelligent Update Manager
generates the list of variable values to transfer and the device loads these values when performing an update. The Intelligent Update Manager
runs each time an application is updated (compiled and downloaded) requiring intelligent updates.Task | Procedure |
|---|---|
Generate a new target snapshot | Generate a target snapshot based on the latest valid compiled application. Before performing an update to a running system where intelligent online updates were not previously enabled, generate a target snapshot for use as a baseline of the current version.
|
Protect a snapshot | Protect a selected historical snapshot from deletion. Protected snapshots do not count towards the number of unprotected snapshots.
|
Unprotect a snapshot | Remove protection from a protected historical snapshot.
|
Set a target snapshot | Set a historical snapshot as the target snapshot when a device is running an earlier application version needing modification.
|
Delete a snapshot | Delete an unprotected target snapshot.
|
Provide Feedback