Intelligent Update Manager Report
The
Intelligent Update Manager
creates an action log each time an intelligent update is required. The log displays when an error occurs or at each compilation when the Always display log...
options are enabled. Since the report only details information about intelligent updates, instances of NO CHANGE display when no change occurred or a minor modification occurred only requiring a regular update. The report does not include changes to variable attributes.Provide Feedback