Branches
Branches create alternative routing for connections. Add parallel branches to elements on a rung. Parallel branch structures display with connections upon clicking a rung.
To perform operations like cutting, copying, pasting, and deleting branches, select a single branch or all branches from a parallel structure. When selecting a single branch, click the connection on the left or right extremity of the branch. The branch connection is highlighted and the branch is outlined. When selecting all branches, click any of the vertical lines joining the branch connections on the left or right extremity of the branches. The branch arm is highlighted and all branches in the structure are outlined.
Single Branch Selection

All Branches Selection

While dragging branches from either the
Toolbox
or within a diagram, the language editor displays the possible drop points. Drop points are display as plus signs in a black circle. For elements, possible drop points display on the rung.Drop points on a rung while dragging elements over the rung

TIP:
When dragging branches, the possible drop points on a
rung display while moving over the rung.
To insert a branch
- From theToolbox, drag the branch element into the language container and place in on the rung where a drop point appears.
- (optional) To reposition a branch within the diagram, select the branch while holding down the left mouse button, then drag the branch to the required location on a rung where a drop point displays.
Provide Feedback