Setting Grid Options

To access the grid options
From the
Tools
menu, click
Options
. In the
Options
dialog box, expand
Grid Settings
, then click the required grid type.
Customize the colors that display in various grids. Access the grid options for the following grids:
  • Arrays View
  • Defined Words View
  • Dictionary View
  • Parameters Grid
  • Structures View
  • Variable Groups View
  • Variable Selector Settings
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal