Variable Groups View

Customize the colors displayed in the Variable Groups view including column headers, row headers, and rows. The Variable Groups view automatically alternates colored rows with white rows. Adjust the number of consecutive rows used for the alternating sequence. The default row coloring scheme is one colored row followed by one white row. For colored rows, define the colors displayed. Also define the color used for the filter and available row, and the color used to indicate disabled rows. For the top left corner of the grid, define the color displayed. Choose whether to display the filter bar in the Variable Groups view.
To customize the colors displayed in the Variable Groups view
  1. From the
    Tools
    menu, click
    Options
    .
  2. From the
    Options
    dialog box, expand
    Grid
    Settings
    , and then click
    Variable
    Groups
    .
  3. Customize the required options, and then click
    OK
    .
    • To specify the number of consecutive rows for the alternating sequence, for
      Consecutive
      Rows
      , indicate the required value.
    • To change the colors applied to headers, alternate rows, disabled rows, the filter/available row, and the top left corner of the grid, click the respective option, and then select a color from the drop-down combo box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal