Arrays View
Customize colors that display in the
Arrays
grid including column headers, row headers, and rows. The Arrays
grid automatically alternates colored rows with white rows. Adjust the number of consecutive rows used for the alternating sequence. The default row coloring scheme is one colored row followed by one white row. For colored rows, define the color to display. Also define the color for the filter, available row, and the color to indicate disabled rows. For the top left corner of the grid, define the color to display. Choose whether to display the filter bar in the Arrays
grid.To customize the display colors in the Arrays grid
- From theToolsmenu, clickOptions.
- From theOptionsdialog box, expandGridSettings, and then clickArrays.
- Customize the required options, and then clickOK.
- To specify the number of consecutive rows for the alternating sequence, forConsecutiveRows, indicate the required value.
- To change the colors applied to headers, alternate rows, disabled rows, the filter/available row, and the top left corner of the grid, click the respective option, and then select a color from the drop-down combo box.
Provide Feedback