Parameters Grid
Customize the colors that display in Parameters grid including column headers, row headers, and rows. The Parameters grid automatically alternates colored rows with white rows. Adjust the number of consecutive rows used for the alternating sequence. The default row coloring scheme is one colored row followed by one white row. For colored rows, define the colors displayed. Also define the color used for the filter and available row, and the color used to indicate disabled rows. For the top left corner of the grid, define the color displayed. Choose whether to display the filter bar in the Parameters grid.
To customize the colors displayed in the Parameters grid
- From theToolsmenu, clickOptions.
- From theOptionsdialog box, expandGridSettings, and then clickParameters.
- Customize the required options, and then clickOK.
- To specify the number of consecutive rows for the alternating sequence, forConsecutiveRows, indicate the required value.
- To change the colors applied to headers, alternate rows, disabled rows, the filter/available row, and the top left corner of the grid, click the respective option, and then select a color from the drop-down combo box.
Provide Feedback