Reset Container and Shape Settings in FBD POUs
Reset the container or shape settings to modify the visual properties for the language containers or elements in Function Block Diagram (FBD) Program Organization Units (POUs).
After resetting the
Container
Settings
in the Properties
window, subsequent elements added to the language editor use the new values.
TIP:
Changes to the
Display
Grid
property made from the Properties
window immediately appear in the language editor.To reset container and shape settings in FBD POUs
- In an open FBD Program Organization Unit (POU), right-click in the language editor, and then select one of these commands:
- ResetContainerSettings -Resets the values defined for theContainer Settingsin thePropertieswindow to the values set inTools>Options>IEC Languages>Function Block Diagram (FBD). Elements in the open POU are not modified.
- Reset Shapes Settings -Resets the visual properties of all elements in the open POU to the properties defined for theContainer Settingsin thePropertieswindow.
- Reset All Settings -Resets the values defined for theContainer Settingsin thePropertieswindow and the visual properties of all elements in the open POU to the values set inTools>Options>IEC Languages>Function Block Diagram (FBD).
To reset shape settings for selected elements in FBD POUs
- In an open FBD POU, select the elements to reset, right-click and then selectReset Shape Settings.The visual properties of the selected elements reset to the values defined for theContainer Settingsin thePropertieswindow.
Provide Feedback