Function Block Diagram Settings
Customize the display settings for Function Block Diagram (FBD) diagrams.
- Choose the comment position for variables.
- Choose whether to display instance names for function blocks.
- Define the colors used to display FBD elements and text and define the variable information that displays in FBD diagrams.
- Choose the width for FBD elements in the language container.
- Choose whether to display grid lines inside FBD language containers.
- Choose to display links as arrows, present solid, dashed, dotted, dashed-dotted, dashed-dotted-dotted, or custom line styles, and apply a normal, rounded, or rounded with jump line types.
Options for customization are:
Option | Description |
|---|---|
Block Style | |
Background Color | The function and function block background color. Possible colors are custom, web, and system colors. |
Background Gradient Color | The function and function block background gradient color. Possible colors are custom, web, and system colors. |
Cell Width | The width for a function or function block, in number of grid cells. |
Display Instance Names | The indication of whether to display instance names for function blocks. |
In design mode, go to definition on double click | While in design mode, enables going to the definition on double click. |
Transparency | The level of transparency. The possible values range from 0 to 255 where 0 indicates complete transparency. |
Comment Style | |
Background Color | The comment background color. The possible colors are custom, web, and system colors. |
Constant Style | |
Background Color - Events | The constant background color. The possible colors are custom, web, and system colors. |
Background Gradient Color - Events | The constant background gradient color. Possible colors are custom, web, and system colors. |
Cell Width | The width for a constant, in number of grid cells. |
Comment Position | The position of the comment in reference to the constant shape. Possible positions are none, top, bottom, left, and right. |
Transparency | The level of transparency. Possible values range from 0 to 255 where 0 indicates complete transparency. |
Variable Information | The information to display for variables. Possible values are name, alias, name and alias, or name and wiring. |
Container Settings | |
Auto Resize Elements when Modifying | When modifying, automatically resize blocks and variables to accommodate length of text. |
Automatically Invoke Variable/Block Selector | Controls whether the Variable or Block Selector is automatically displayed when inserting a variable or block in the language container. |
Display Grid | Determines whether to display the grid in the language container. |
Event Link Style | |
Arrow | Determines whether to display an arrow at the end of the link. |
Line Style | The style of the line. Possible values are solid, dash, dot, dash-dot, dash-dot-dot, and custom. |
Line Type | The type of line. The normal line type has squared corners and overlapping link intersections. The rounded line type has rounded corners and overlapping link intersections. The rounded with jump line type has rounded corners and link intersections are jumped over. |
Link Event Color | The color of event links. Possible colors are custom, web, and system colors. |
Jump | |
Cell Width | The width for a jump, in number of grid cells. |
Label | |
Cell Width | The width for a label, in number of grid cells. |
Left Power Rail | |
Background Color | The left power rail background color. Possible colors are custom, web, and system colors. |
Background Gradient Color | The left power rail background gradient color. Possible colors are custom, web, and system colors. |
Link Style | |
Arrow | Determines whether to display an arrow at the end of the link. |
Line Style | The style of the line. Possible values are solid, dash, dot, dash-dot, dash-dot-dot, and custom. |
Line Type | The type of line. The normal line type has squared corners and overlapping link intersections. The rounded line type has rounded corners and overlapping link intersections. The rounded with jump line type has rounded corners and link intersections are jumped over. |
Link Color | The color of links. The possible colors are custom, web, and system colors. |
Online Settings | |
Online Text Color - Variable and Block | The color of text that displays the value of the variables in online mode and simulation mode. |
Operator Style | |
Background Color | The operator background color. Possible colors are custom, web, and system colors. |
Background Gradient Color | The operator background gradient color. Possible colors are custom, web, and system colors. |
Cell Width | The width for an operator, in number of grid cells. |
Display Instance Names | Determines whether to display instance names for operators. |
In design mode, go to definition on double click | While in design mode, enables going to the definition on double click. |
Transparency | The level of transparency. Possible values range from 0 to 255 where 0 indicates complete transparency. |
Region Style | |
Background Color | The region background color. Possible colors are custom, web, and system colors. |
Header Color | The header color of a region. Possible colors are custom, web, and system colors. |
Header Transparency | The level of transparency of the header section of a region. The possible values range from 0 to 255 where 0 indicates complete transparency. |
Transparency | The level of transparency. Possible values range from 0 to 255 where 0 indicates complete transparency. |
Right Power Rail | |
Background Color | The right power rail background color. Possible colors are custom, web, and system colors. |
Background Gradient Color | The right power rail background gradient color. Possible colors are custom, web, and system colors. |
Variable Style | |
Background Color | The variable background color. Possible colors are custom, web, and system colors. |
Background Gradient Color | The variable background gradient color. Possible colors are custom, web, and system colors. |
Cell Width | The width for a variable, in number of grid cells. |
Comment Position | The position of the comment in reference to the variable shape. Possible positions are none, top, bottom, left, and right. |
Transparency | The level of transparency. Possible values range from 0 to 255 where 0 indicates complete transparency. |
Variable Information | The information that displays for variables. Possible values are name, alias, name and alias, or name and wiring. |
To customize the display settings for FBD diagrams
- From theToolsmenu, clickOptions.
- From theOptionsdialog box, expandIECLanguages, then clickFunctionBlockDiagram(FBD).
Using the available options, customize the required settings, then click
OK
.Provide Feedback