Sequential Function Chart Settings
Customize the display settings for SFC diagrams. Choose the orientation of the pane splitting when displaying SFC diagram and actions/conditions programming simultaneously in the language container. Choose to display grids and sequence control types and diagram background and grid colors for design and online modes. For action blocks, jumps, and transitions, define the background, gradient, and font colors and the font style. For steps, define the active and inactive step and step gradient colors, the font color and style and the action list and list gradient colors.
Options for customization are:
Setting | Description |
|---|---|
Action Block Settings | |
Action Block Color | The background color of action blocks. The possible colors are custom, web, and system colors. |
Action Block Font | The font definition used for the text displayed in an action block. The definition includes the font name, size, unit of measure, and the indication of whether to apply bold, italic, strikeout, and underline styles. The GDI Character Set and GDI Vertical Font properties are not editable. |
Action Block Font Color | The color of the font for action blocks. The possible colors are custom, web, and system colors. |
Action Block Gradient Color | The background gradient color of action blocks. The possible colors are custom, web, and system colors. |
Container Settings | |
Background Color - Design | The background color for SFC diagrams while in design mode. The possible colors are custom, web, and system colors. |
Background Color - Online | The background color for SFC diagrams while online. The possible colors are custom, web, and system colors. |
Container Split Orientation | Controls the orientation for the splitting of the container between the SFC diagram and Actions/Conditions views. The possible values are vertical or horizontal. |
Display Grid | The indication of whether to display the grid. |
Display Sequence Control Type | The indication of whether to display the sequence controls type. |
Display Transition Priority | The indication of whether to display the transition priority. |
Grid Color - Design | The color of the grid while in design mode. The possible colors are custom, web, and system colors. |
Grid Color - Online | The color of the grid while running online. The possible colors are custom, web, and system colors. |
Jump Settings | |
Jump Color | The background color of jumps. The possible colors are custom, web, and system colors. |
Jump Font | The font definition used for the text displayed in a jump. The definition includes the font name, size, unit of measure, and the indication of whether to apply bold, italic, strikeout, and underline styles. The GDI Character Set and GDI Vertical Font properties are not editable. |
Jump Font Color | The color of the font for jumps. The possible colors are custom, web, and system colors. |
Jump Gradient Color | The background gradient color of jumps. The possible colors are custom, web, and system colors. |
Macro Call Settings | |
Macro Call Color | Not supported |
Macro Call Font | Not supported |
Macro Call Font Color | Not supported |
Macro Call Gradient Color | Not supported |
Step Settings | |
Action List Color | The background color of action lists. The possible colors are custom, web, and system colors. |
Action List Gradient Color | The background gradient color of action lists. The possible colors are custom, web, and system colors. |
Step Color | The background color of steps. The possible colors are custom, web, and system colors. |
Step Color - Active | The background color of active steps while online. The possible colors are custom, web, and system colors. |
Step Font | The font definition used for the text displayed in a step. The definition includes the font name, size, unit of measure, and the indication of whether to apply bold, italic, strikeout, and underline styles. The GDI Character Set and GDI Vertical Font properties are not editable. |
Step Font Color | The color of the font for steps. The possible colors are custom, web, and system colors. |
Step Gradient Color | The background gradient color of steps. The possible colors are custom, web, and system colors. |
Step Gradient Color - Active | The background gradient color of active steps while online. The possible colors are custom, web, and system colors. |
Transition Settings | |
Transition Color | The background color of transitions. The possible colors are custom, web, and system colors. |
Transition Font | The font definition used for the text displayed in a transition. The definition includes the font name, size, unit of measure, and the indication of whether to apply bold, italic, strikeout, and underline styles. The GDI Character Set and GDI Vertical Font properties are not editable. |
Transition Font Color | The color of the font for transitions. The possible colors are custom, web, and system colors. |
Transition Gradient Color | The background gradient color of transitions. The possible colors are custom, web, and system colors. |
To customize the display setting for SFC diagrams
- From theToolsmenu, clickOptions.
- From theOptionsdialog box, expandIECLanguages, then clickSequentialFunctionChart.
- Using the available options, customize the required settings, then clickOK.
Provide Feedback