Properties Window
To access the Properties window
From the View menu, click
Properties Window
. The F4
or Alt+Enter
keyboard shortcuts are also available.Use the
Properties
window to view and edit the properties of items selected within language containers, the Application View
, and other various views. Also use the Properties
window to view and edit file and project properties. View the common properties for multiple objects and elements. When selecting multiple objects, the Properties
window displays only the properties that are common to all the objects and elements.In the
Properties
window, properties are organized alphabetically or into categories displayed alphabetically. Expand the categories to view the property information including property names and values. Properties that display in gray are read-only.Edit property values using the plain text fields and drop-down combo boxes provided. Where required, links to custom editors or dialog boxes displayed in the property value fields.
The Properties window toolbar contains:
Icon | Description |
|---|---|
![]() | Displays the name of the item or group of items selected. |
![]() | Displays the property names and values organized into categories. |
![]() | Displays the properties sorted in alphabetical order |
![]() | Not applicable |
Provide Feedback