Description Window
To access the Description window
- From theViewmenu, selectDescription Window.
Use the
Description Window
to add descriptions to projects, program organization units (POUs), and AADvance controllers. These descriptions are free-formatted text using rich text format (RTF). All content is automatically saved. When editing descriptions, a text editor toolbar provides the means for performing basic formatting operations like selecting a font, size, style, and color.The
Description Window
is dockable and scalable. The contents of the Description Window
automatically displays the description for items selected in the Application View
.
TIP:
While in debug mode, the content in the Description Window is read-only.
Provide Feedback