Devices

Devices are the modules, drives, controllers, HMI panels, computers, CIP Proxy devices,
OPC UA
servers, and
OPC UA
clients that work together to create a
FactoryTalk
system.
TIP: Add devices that share security requirements and that should trust each other to a zone. A device can have one or more ports that are added to the policy model. Connect devices to other devices or zones with conduits.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal