Ports

A port represents a physical socket of a device that allows communication with another device.
TIP:
FactoryTalk Linx
Devices, CIP Proxy devices, and
Rockwell Automation
devices that are identified by catalog number have only a single port. CIP Proxy devices and proxied devices have an additional section in
PORT PROPERTIES
indicating the paired device.
Add ports to Generic Devices to add them to the security policy model.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal