Delete a port

Delete not needed ports from devices.
Prerequisites
Confirm that the device has more than one port configured.
  1. From the navigation bar, either:
    • Select
      Canvas
      and then select a device.
    • Select
      Zones
      and then select a zone and a device.
    • Select
      Devices
      and then select a device.
  2. In
    Properties
    , under
    Ports
    , next to the port to delete, select
    Delete
    .
  3. Select
    DELETE
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal