Move a device

You can move devices in the
Canvas
policy model visualization and in the
Graphical Explorer
tree.
TIP: You can also move a device by editing the device properties. See Edit a device.
  1. From the navigation bar, either:
    • Select
      Canvas
      .
    • Select
      Zones
      and then select a zone.
    • Select
      Devices
      .
  2. Right-click a device and select
    Cut
    .
  3. Right-click the blank space and select
    Paste
    .
    TIP:
    You can paste the device to a different zone or to the list of unassigned devices. Switching between
    Canvas
    ,
    Zones
    , and
    Devices
    does not discard the copied device.
    In
    Canvas
    , you can drag devices between containers. You can also drop devices from the
    Graphical Explorer
    tree to the
    Canvas
    policy model visualization or in the opposite way.
    IMPORTANT: In
    Canvas
    , when you move a device from the
    Onboarding Area
    to a
    Zone
    or to the
    Unassigned
    container, the device cannot be moved to the
    Onboarding Area
    container again.
The device is moved to another zone. The
OPC UA
client and
OPC UA
server pair moves together.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal