Duplicate a device

Copy and paste a device to duplicate the device with its properties.
  1. From the navigation bar, either:
    • Select
      Canvas
      .
    • Select
      Zones
      and then select a zone.
    • Select
      Devices
      .
  2. Right-click a device and select
    Copy
    .
  3. Right-click blank space and select
    Paste
    .
    TIP: You can paste the device to the same zone, a different zone, or to the list of unassigned devices. Switching between
    Canvas
    ,
    Zones
    , and
    Devices
    does not discard the copied device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal