Traces tab

How do I open the Traces tab?
Click the trend chart on the screen, and in the
Properties
pane, click the
Traces
tab.
Use traces to visually display values on a trend chart. Each trace represents a set of data points collected over time.
Use the
Traces
tab to:
  • Add or delete traces on a trend chart.
  • Bind to a tag, user-defined property, or property of a graphic element containing the data to depict on the trace.
  • Change the appearance of a trace.
  • Label a trace for diagnostic purposes.
For example, using the
Traces
tab, add a blue trace to monitor the pressure of water filling a tank and a red trace to monitor the temperature of the water. The resulting trend chart shows, in real-time, the current water pressure and water temperature for the tank.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal