Delete a trace from a trend chart

Delete a trace from a trend chart to no longer display the values associated with the trace on the trend chart. For example, delete a trace if its data depicts a bottling line being discontinued from the manufacturing system.
To delete a trace from a trend chart
  1. Select the trend chart on the screen.
  2. In the
    Properties
    window, select the
    Traces
    tab.
  3. In the upper right corner of the
    Trace
    card of the trace to delete, select
    Delete Trace
    Designer Delete icon. The trace no long appears on the trend chart.
    TIP:
    Deleting a trace does not delete the tag from a data log.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal