Remote LCD overview
The 2080-Remote LCD is an external device that you can attach to the following controllers using an embedded serial port:
- L20E controllers
- L50E controllers
- L70E controllers
To configure and program the Remote LCD settings, use the Remote LCD configuration page, and the LCD_REM, KEY-READ-REM and LCD_BKLT_REM function blocks.
For more information about the 2080-Remote LCD and the wiring instructions, see Micro820 Programmable Controller User Manual (publication 2080-UM005).
Provide Feedback