Remove remote LCD overwrite for serial port settings
By default, remote LCD settings overwrite the Common Industrial Protocol settings configured on the
Serial Port
configuration page for L20E controllers that support remote LCD.Clear the
Configure the serial port for remote LCD
checkbox to remove the remote LCD overwrite for serial port settings.To remove remote LCD overwrite for serial port settings
- InProject Organizer, double-click the controller to open the controller application workspace.
- In theControllertree, selectRemote LCD.
- On theRemote LCDconfiguration page, clear theConfigure the serial port for remote LCDcheckbox.
- Select theserial portlink to open theSerial Portconfiguration page, and then configure the serial port settings as needed.
Provide Feedback