Admin
The
Admin
tab contains components that require administrative privileges. You need to log on to open it. The default user name and password are admin/admin
.The administrator session expires after 20 minutes, however, it is renewed each time you act on the
Admin
tab or each time you access other tabs on the FactoryTalk Historian ME Web Diagnostics page and/or perform actions there. If your session expires on the Admin
tab, you will be automatically logged out and taken to the Home
tab.
TIP:
For security reasons, we recommend that you log out of the FactoryTalk Historian ME Web Diagnostics when you finish working with it.
The tab contains the following information:
- TIP:If you want to simultaneously log in to the web diagnostics clients for multiple FactoryTalk Historian ME modules, note the following:
- If you are using Internet Explorer (compatibility mode), logging out of one tab from a single Internet Explorer session causes all other logged-in tabs to log out as well.
- If you are using Internet Explorer (compatibility mode), logging out of one session will also trigger the other logged-in sessions to log out as well.For either of these scenarios, if you get logged out unexpectedly, log back in to the tab you want to view.
Provide Feedback