PI commands
IMPORTANT:
Executing some PI commands can irreparably damage the data server, stored data, and possibly the FactoryTalk Historian ME module. Consult with Rockwell Technical Support before executing any PI command.
The
PI commands
page lists all available PI commands.If the
Options
text box remains blank and you click Execute
, a list of valid PI options will appear. To execute a command, type the command in the Options
text box and click Execute
.
TIP:
When the FactoryTalk Historian ME module is in Safe Mode, PI commands cannot be executed. For details on how to get the module out of Safe Mode, see Repair archives using safe mode.
Provide Feedback