Repair archives using safe mode
Each time you reboot the system, the system checks to see if your archive files contain any
data that has a timestamp for a time in the future. If future timestamps are found upon
rebooting, the module's STS light is solid red and the LED displays either
SAFE MODE
LAN OK <IP_address>
or SAFE MODE LAN LOST
<MAC_address>
. Both messages indicate that the module is in safe mode. When
this happens, the module web interface is inaccessible and you must go to the Web
Diagnostic
page to repair the archive files. When the module is in safe mode, PI
commands cannot be executed.When the module is in safe mode, the following error message appears on the
Web Diagnostics
page:ERROR: Archives are in inaccessible state. Please navigate to "Safe Mode" or click on "Repair" to continue.
To access the bad archives information, follow the message instructions.
The bad archives are listed and selected by default.
You can repair the bad archives by repairing the time setting. For details, see Repair the time setting.
Provide Feedback