Repair the time setting
To repair the time setting
- On theSafe Modepage, select theRepair Timeoption.
- In theTimetext box, type the correct time.
- Choose the time zone and the region from the provided lists.
- ClickChange Time. A message appears:INFO: The time sync is successful. Please wait while system reboots...
- Wait for the module to reboot. The archives have been repaired.IMPORTANT:If you choose to repair time, be aware that if you have previously synchronized your ME module to an external time source such as a controller or an NTP server, clicking Repair Time will reset your time source to manual. We recommend, therefore, that before you perform this step, you attempt to fix the problem with your original time source first. For details, see Manage time.TIP:If you do not want to repair the time, you can wait until the time listed in the timestamp is no longer in the future. Once that occurs, click Reboot to reboot the module. When the archives are checked again, no future timestamps will be found in the archive files and no repair is needed.
Provide Feedback