Download logs
IMPORTANT:
Any kind of firmware upgrade or reinstallation will clear out all logs. A firmware upgrade will preserve archived data and application configuration information, but a reinstallation will clear out all application configuration information and archived data. If you want to save your settings, download and back up your configuration and logs.
The
Download Logs
page contains the name of the existing packaged log file, the time when it was packaged, and the size of the file. Use the provided buttons to package log files, download packaged log files, and delete packaged log files.After the packaged logs are downloaded, the packaged export can be deleted so that it does not utilize space on the FactoryTalk Historian ME module. The original log files are not deleted.
Provide Feedback