Hosts
The
Hosts
page lists the contents of the module's hosts file. The hosts file can be
used to provide hostname-to-IP address resolution for networks that do not have reliable DNS
servers available.Use this page to do the following:
- To add a new host, clickNew. Type the new hostname and IP address and clickSave.
- To edit a host, select the host in the list and clickEditto make theHost NameandIP Addressbars editable. Update the host name and IP address, and clickSave.
- To delete a host, select the host in the list and clickDelete. You will be asked to confirm the deletion. ClickOKto delete the host.
Provide Feedback