Use the Rule Editor
FactoryTalk Historian ME Rule Editor is a component of the FactoryTalk Historian ME Client Tools suite. You can use it to create, edit, and delete custom rules for the point discovery process. The selections you make in the dialog box are automatically written to the point discovery rule file. After you create rule files, you can upload them to the module with the upload manager (see Upload files to the module). Tags that match the rules that you create will be found and added to the FactoryTalk Historian ME server as part of the tag discovery process (see Add points using the Add Points Wizard page).
With the Rule Editor, you can perform the following:
Provide Feedback