Upload files to the module
To upload a file to the FactoryTalk Historian ME Module
- Click theAdvancedtab, and then clickUpload Management.TheUpload Managementpage appears.
- In theFile Typelist, select the file type.For details on the file types you can select, see File types.
- In thePlease Select Filebox, type the file name, or clickBrowseto locate the file.The file name may only contain the following characters:@, ., -, _, a-z, A-Z, 0-9, and must not contain any spaces.
- ClickUpload To Moduleto upload the selected file to the module.The uploaded file is displayed in the table. The table includes the name, type, and size of the file, as well as the time the file was last modified.TIP:Files of typeCa Certificate,Server Certificate, andPrivate Keymust have the.pemextension. Files of typeAutoDiscoveryRuleFile,TagAttributeFile, andUser-defined Timeoutsmust have the.xmlextension.The maximum size of the file you want to upload may not exceed 500 KB.If you use HTTPS, do not delete files of the typeCA Certificate,Server Certificate, andPrivate Keyafter uploading them.For details on security settings, see Manage security.
Provide Feedback