Manage security

Security of the FactoryTalk Historian ME module is managed on the
System Security
page. To access the
System Security
page, click the
Configure Historian
tab, and then click
System Security
.
Any changes to module security settings will automatically log out the current user because the users and user groups available depend on the security mode selected. Changing the security mode will also cause the module to reboot. This process may take a few minutes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal