Integrate the module into a FactoryTalk environment with FactoryTalk Directory

In this section, you will learn how to integrate a standalone FactoryTalk Historian ME module into an existing FactoryTalk system using FactoryTalk Directory. Integrating a standalone module into an existing FactoryTalk system allows:
  • Centralized administration of security credentials, performed in FactoryTalk Administration Console.
  • FactoryTalk clients (for example, FactoryTalk View SE or FactoryTalk Batch) to connect to the FactoryTalk Historian ME module.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal