Integration prerequisites
Before you register the module in FactoryTalk Directory from a client computer, ensure that:
- The FactoryTalk Services Platform is installed and configured on the client computer.
- FactoryTalk Historian ME Management is installed on the client computer.
- You are using the FactoryTalk Directory security credentials to log on to the module. For details, see Configure how to log on to the module.
Provide Feedback