Register the module in the FactoryTalk Directory
You can register the FactoryTalk Historian ME module in the FactoryTalk Directory using the FactoryTalk Administration Console. To register the module, you must create an initial server connection.
TIP:
For a list of prerequisites needed to use the FactoryTalk Directory, see Log on using the FactoryTalk Directory with FactoryTalk Historian ME.
Provide Feedback