Add the Historian ME module in the PI SDK Utility

To add the Historian ME module in the PI SDK Utility
  1. Go to
    Start > All Programs > Rockwell Software > FactoryTalk Historian SE > FactoryTalk Historian SE System > About PI-SDK
    .
    The
    PI SDK Utility
    window appears.
  2. On the
    File
    menu, click
    Connections
    .
    The
    PI Connection Manager
    dialog box appears.
  3. On the
    Server
    menu, click
    Add server
    .
    The
    Add PI Server
    dialog box appears.
  4. In the
    Network Path/FQDN
    box, type the IP address of the Historian module.
  5. Click
    OK
    .
    If a connection was successfully established, the IP address will appear in the
    PI Connection Manager
    dialog box. If an error occurs, the module might be restarting. Ensure that the middle STS LED is flashing green on the module. This indicates that the module has fully initialized and a connection can be established.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal