SNMP community strings

The Simple Network Management Protocol (SNMP) is a protocol for communication between devices connected in a network. SNMP uses community strings as passwords that allow a get-request to access the statistics of a module.
TIP:
  • The Backup and Restore function does not include the SNMP community strings.
  • Restoring FactoryTalk Historian ME defaults disables SNMP and deletes the existing community strings. The system creates the default community string:
    public
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal