Create SNMP community strings

Create SNMP community strings to use them as passwords to enable access to a device's statistics.
TIP:
  • Only accounts with piadmin or FTHAdministrators privileges can modify the contents of
    SNMP Management
    page.
  • While SNMP is enabled, it is not possible to add or delete community strings.
  • The string can contain up to 35 alphanumeric characters (A-Z, a-z, 0-9).
  • FactoryTalk Historian ME supports a maximum of 5 community strings.
To create SNMP community strings
  1. Select the
    Advanced
    tab, then select
    SNMP Management
    .
  2. Uncheck the
    Enable SNMP
    checkbox.
  3. Select
    Create
    .
  4. In the next screen, enter the community string.
  5. Select
    Save
    .
  6. Repeat steps 3-5 as needed.
  7. Recheck the
    Enable SNMP
    checkbox.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal